DOCA0147EN-17

Firmware Version 004.011.000

New Features

The following events are added with email notification:

  • Events from the IDMTG ground-fault protection.

  • Events indicating the change of passwords.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?