DOCA0147EN-17

Firmware Version 003.013.003

New Features

The new range of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers are introduced with the evolution of existing ComPact NSX and PowerPact H-, J-, and L-frame range of circuit breakers.

Bugs Fixed

New administrators were able to perform the control operations without the acceptance of the disclaimer message.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?