DOCA0147EN-17

Firmware Version 004.002.000

New Features

  • Added MicroLogic Xi control units. A MicroLogic Xi is a control unit without Bluetooth Low Energy (BLE) communication.

  • Enhanced the following cybersecurity features:

    • Enabled the FTPS mode for file import.

    • Enabled automatic export of datalog file.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?