DOCA0147EN-17

Firmware Update Policy

Firmware update is recommended to benefit from the latest features and potential bug fixes. Do not update the firmware to the latest version, if the latest features are not required for your application and no bug fixes are provided.

Use this release note to confirm if an update to the latest version of the firmware is relevant for your application.

NOTE: You can upgrade the firmware version from 003.nnn.nnn to 005.nnn.nnn and 004.nnn.nnn to 005.nnn.nnn but downgrade is not possible.

For more information on the firmware update policy and the firmware compatibility between devices, refer to MicroLogic Trip Units and Control Units - Firmware HistoryDOCA0155EN.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?