Status screens
Summary
The default screen shows the summary screen. This screen displays uncommissioned channels, commissioned channels, and insulation status of the commissioned channels.
An example of all 12 commissioned channels is as follows:
An example of 12 commissioned channel and 3 channels (channel number : 2, 6, and 10) displaying insulation alarm is as follows:
An example of 12 commissioned channel and 3 channels (channel number : 2, 6, and 10) displaying acknowledged insulation alarm is as follows:
Insulation resistance measurement (R)
The device displays the insulation resistance measurement of each individual channel. An example measurement of channel 4 is as follows:
Impedance measurement (Z)
The device displays the impedance measurement of each individual channel. An example measurement of channel 4 is as follows:
Insulation alarm detected: insulation fault
The device displays the insulation fault screen when the insulation value falls below the insulation alarm threshold. An example of insulation alarm of channel 4 is as follows:
There are two possible scenarios:
Insulation alarm acknowledged
This screen is displayed when you have acknowledged the insulation alarm. An example of insulation alarm acknowledged of channel 4 is as follows:
Transient fault
This screen is displayed when a transient fault has occurred. An example of transient alarm of channel 4 is as follows: