7EN02-0423-03

Modbus functions

The device supports Modbus function codes.
The following table is profiled. Check for profiling before editing.
Function Code Function Name
Decimal Hexadecimal
3 0x03 Read Holding Registers *
4 0x04 Read Input Registers *
6 0x06 Write Single Register
8 0x08 Diagnostic Modbus
16 0x10 Write Multiple Registers
43 / 14 0x2B / 0E Read Device Identification
43 / 15 0x2B / 0F Get Date/Time
43 / 16 0x2B / 10 Set Date/Time
98 0x62 Modbus/98 *

Read Device Identification request

Number Type Value
0 VendorName

Schneider Electric

1 ProductCode IMDIM400N / IMDIM400THRN
2 MajorMinorRevision XXX.YYY.ZZZ
3 VendorURL

www.se.com

4 ProductName Insulation Monitoring Device
5 ModelName IM400N / IM400THRN

The device answers any type of requests (basic, regular, extended).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?