7EN02-0423-03

Injection inhibition screen

When the injection inhibition function is activated (that is, Inhibit. Input is set to N.O.), the following status screen displays and replaces any system status screen that may be displaying already (insulation measurement, insulation alarm or preventive insulation alarm).

You can perform the following actions on this screen:

  • Press the Menu button to go to the main menu.

  • Press the arrow buttons to view the settings screen.

  • Press the T button to run the auto-test.

NOTE:

If you activate the injection of the device,

  • If Inhibition Type value is Int., then an auto test is launched automatically before returning to the default insulation monitoring screen.

  • If Inhibition Type value is Ext., then the device displays the default insulation monitoring screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.