7EN02-0477-02

Test with relays (Test w. Relays)

You can set a three-second toggle to the insulation alarm relay during a manually launched auto test. See Auto test overview for information on auto test.

The allowed values for this parameter are ON and OFF. The default value is ON.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?