7EN02-0477-02

Commissioning

The MFLK1 can be commissioned in two ways depending on the voltage input connection with the system.

It is dependent on the following two criteria:

  • When voltage input is connected to the system

  • When voltage input is not connected to the system

When voltage input is not connected to the system, perform the following steps:

  1. Configuring IMD and MFLK1

  2. MFLK1 is not connected to the system voltage: Calibrating the MFLK1 and locating the fault

When voltage input is connected to the system, perform the following steps:

  1. Configuring IMD and MFLK1

  2. MFLK1 is connected to the system voltage: Locating the fault

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?