7EN02-0477-02

Safety precautions

Installation, wiring, testing and service must be performed in accordance with all local and national electrical codes.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate Personal Protective Equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or other local standards.
  • Assume communications and I/O wiring are hazardous live until determined otherwise.
  • Do not exceed the maximum ratings of this device.
  • Never shunt an external fuse or circuit breaker.
  • Battery is not user replaceable. MFLK1 should not be opened by user, once opened warranty is void. User should contact Schneider customer care for any issues.
  • Ensure that your ungrounded system has a compatible insulation monitoring device.
  • Ensure that your ungrounded system voltage is less than 230 V.
Failure to follow these instructions will result in death or serious injury.
NOTE: See IEC 60950-1, Annex W for more information on communications and I/O wiring connected to multiple devices. See IEC 60364-4-41 for more information on protection against electrical shock.
WARNING
Unintended Operation
Do not use this device for critical control or protection of persons, animals, property or equipment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
Equipment damage
  • Do not open the front panel.
  • Do not attempt to repair any components of the device.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?