7EN02-0477-02

Reset

You can reset logs and trends. Further, you can perform factory reset.

You can access the device reset parameters by selecting Menu > Settings > Reset.

The reset parameters are Reset Logs, Reset Trend, and Factory Reset.

On performing reset of logs or trends, the existing logs or trend information is erased but the settings parameter value remains unchanged. On performing factory reset, the device restarts and the settings parameter values are reset to default.

The complete list of parameter settings, its default value, and allowed values are:

The following table is profiled. Check for row profiling before making any content change.
Parameter Default Value Allowed Values
Ins. Alarm 10 kΩ 0.2...200 kΩ
Ins. Al. Relay FS
  • FS

  • Std.

Modify Password 0000 0000...9999
Activation (Password) OFF
  • ON

  • OFF

Contrast 50% 10...100%
Backlight 100% 10...100%

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?