7EN02-0477-02

Configuring IMD and MFLK1

Whenever a fault is identified by the IM400 or XGR device, perform the following:
  1. Unlock and open the MFLK1.
  2. Turn ON the power switch.
    Check the available battery capacity displayed in Battery Display.
  3. If IMD monitors the system, it has to be set in Power C or Control C mode. Photovolt mode is not compatible.
    1. MFLK1 setting:
      • MENU > Settings > Network > Inj.Device must be set to IM400

      • MENU > Settings > Network > App. must be set to same as IMD.

  4. If XGR monitors the system:
    1. MFLK1 setting: MENU > Settings > Network > Inj.Device must be set to XGR.
NOTE: See the IM400 or XGR User Manual for more information on modifying parameters.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?