MFLK1 is not connected to the system voltage: Calibrating the MFLK1 and locating the fault
- Open the CT connector cap.
-
Connect the CT probe to its specific cable and quarter turn the CT probe connector.NOTICE Equipment damage- Ensure that CT probe cable is connected to the CT connector.
- Ensure that voltage input cable is connected to the voltage input connector.
Failure to follow these instructions can result in equipment damage. - Clamp the CT probe as closely as possible to the injection terminal of the IM400 or XGR.
- Press the Calibration button.The Launch Calibration? message displays.
- Press the Confirm button.The calibration begins and then displays the percentage of current, which is the reference for all other measurements downstream.
-
NOTE: Fault will be located by checking the relative current flow in percentage.Clamp the CT probe to the first level of feeders.
-
If the percentage of the current is very low compared to others, then there is no fault in this feeder, continue to check the next downstream feeders.
-
If the percentage of the current is high low compared to others, then there is fault in this feeder, should be disconnected and repaired.
-