7EN02-0477-02

Injection Device(Inj. Device)

The device supports IM400 series and XGR injection devices. You can select the required injection device of the network, so the device can measure the relative current flow or the insulation resistance (when locating signal is available).

Two values are available for this parameter:

  • IM400

  • XGR

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?