Hardware overview
| A | CT probe connector: To connect the MFLK1 to the appropriate open core toroid.* | |
| B | Voltage input probe connector: (If required) To connect the MFLK1 with the system voltage, between line and earth.* | |
| C | Battery charge level: Displays the available battery capacity (Alternatively in percentage and in Volts). | |
| D | Red LED and buzzer: When the MFLK1 detects insulation fault, LED turns ON and the buzzer is activated. | |
| E | Power connector: To charge the MFLK1.Use CE/IEC certified charger having output ratings 24 V DC, 1 A. | |
| F | Fault
locator display: Displays
|
|
| G | Power ON/OFF switch | |
| H | CT connector with cap: To connect the MFLK1 to the CT probe. | |
| I | Voltage input connector with cap: (If required) To connect the MFL to the Voltage Input Probe. |
Device commercial reference
| Model | Commercial reference |
|---|---|
|
MFLK1 |
IMDMFLK1 |