7EN02-0477-02

Filtering

You can set the filtering parameter as per the monitored application.
Value Response time Advised Usage
5s 5 seconds

Use in maintenance mode.

Diagnose fast variation of the insulation resistance and leakage capacitance.

Use in the following cases:

  • Detecting short time transient insulation faults.

  • When manually locating insulation faults by opening circuit breakers.

40s (Default) 40 seconds

Use in operation mode.

To monitor insulation of typical installations.

400s 400 seconds

Use in operation mode.

To monitor insulation of highly disturbed installations and/or installations with high leakage capacitance.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?