7EN02-0477-02

Frequency

You can set the rated frequency of the monitored application.

  • 50 Hz (by default)

  • 60 Hz

  • 400 Hz

  • DC

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?