7EN02-0477-02

Alarm configuration

You can configure the insulation alarm threshold and delay to suit to the electrical applications you want to monitor.

You can access the device alarm parameters by selecting Menu > Settings > Ins.Alarm.

By default, the alarm parameter is Ins. Alarm%, meaning the Locating Signal parameter is OFF.

When the Locating Signal network parameter is ON, then the alarm parameters are Ins. Alarm and Ins. Al. Delay.

To modify the parameter value, see IFL parameter modification using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?