7EN02-0477-02

Relative insulation alarm threshold (Ins. Alarm%)

You can set the threshold value versus the calibration level.

The allowed values for this parameter are 50%, 60%, 70%, 80%, and 90% of the calibrated signal. The default value is 50%.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?