7EN02-0477-02

Network configuration

You can configure the electrical network parameters to suit the electrical applications you want to monitor.

You can access the device network parameters by selecting Menu > Settings > Network.

The network parameters are:

  • Inj. Device

  • App

  • Locating Signal

  • Filtering

  • Frequency

  • V.Adapt

To modify the parameter value, see IFL parameter modification using the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?