7EN02-0477-02

Locating Signal

You can set the locating signal parameter as per the monitored application.

The allowed values for this parameter are Yes and No. The default value is No, meaning the MFLK1 is not connected to the system's voltage, then the device measures and displays the relative current flow.

When locating signal is available, set the parameter value to Yes so the device measures and displays the insulation resistance and capacitance.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?