7EN02-0477-02

Insulation measurements

The device monitors the insulation of ungrounded power system.

By default, the device measures and displays the relative current flow in percentage.

When locating signal is available, the device:

  • measures and displays:

    • the insulation resistance R (Ω) continuously,

    • the insulation capacitance C, which is the leakage capacitance of the distribution system to ground (μF),

  • calculates and displays the impedance Zc (kΩ) associated with C.

To view these values, navigate to Menu > Monitoring.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?