De-Energizing the Device
Isolation Capacity
TeSys GV5 / GV6 devices offer positive contact indication and are suitable for isolation in accordance with IEC/EN 60947-1 and 2 standards. The O (OFF) position of the actuator is sufficient to isolate the device concerned.
The following marking on the rating plate
label indicates that the device is capable of isolation: 
To confirm this capability, IEC/EN 60947-1 and 2 standards require specific shock withstand tests.
TeSys GV5 / GV6 devices can be locked in the O (OFF) position to allow work to be carried out with the power off in accordance with installation rules. The device can only be locked in the open position if the device is in the O (OFF) position.
Maintenance and Servicing Work on Installation
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Turn off all power supplying the equipment before working on or inside equipment. For a partial powering down of the installation, the installation and safety rules require clearly labeling and isolating the feed being worked on.
Maintenance Work Following a Trip on Electrical Fault
WARNING |
|---|
|
HAZARD OF CLOSING ON ELECTRICAL FAULT
Do not close the device again without first inspecting
and, if necessary, repairing the downstream electrical equipment.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The following table describes the procedure to be followed after a trip on electrical fault:
|
Step |
Action |
|---|---|
|
1 |
Isolate the feed before inspecting the downstream electrical equipment. |
|
2 |
Look for the cause of the detected fault. |
|
3 |
Inspect and, if necessary, repair the downstream equipment. |
|
4 |
Inspect the equipment in the event of a short-circuit trip. |
|
5 |
Close the device again. |
Checking the Settings
Checking settings does not require any particular precautions. The checks must be carried out by a qualified person.
Testing the Device
CAUTION |
|---|
|
HAZARD OF NUISANCE TRIPPING
Protection tests must be done by qualified electrical
personnel.
Failure to follow these instructions can result in injury or equipment damage.
|
When testing device trip mechanisms, precautions must be taken:
-
To avoid disrupting operations.
-
To avoid inappropriate actions or tripping of alarms.
For example, tripping the device with the push-to-trip button can lead to inappropriate fault indications or corrective actions (such as switching to a replacement power source).
Setting the Trip Unit
WARNING |
|---|
|
HAZARD OF NUISANCE TRIPPING OR FAILURE TO TRIP
Protection setting adjustments must be done by qualified
electrical personnel.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Modifying trip unit settings requires a thorough knowledge of the installation and safety rules.
DANGER
WARNING
CAUTION