DUG_16A Connected Switch-01

Reassigning the device to a room

You can reassign a device to a room using the Wiser app.

To reassign:

  1. On the Devices page, tap Rooms.
  2. Select the room.
  3. Tap + (A) to add a device.
  4. Select a device from the Devices list.
    NOTE: When you turn the room on/off (B), the devices that have been added to that room are activated.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?