DUG_16A Connected Switch-01

Removing devices from favourites

You can remove devices from the favourites list using the Wiser app.

To remove favourities:

  1. On the Dashboard page, tap Edit (A).
    The Manage Favourites page appears.
  2. Unselect the device.
  3. Tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?