DUG_16A Connected Switch-01

Pairing the device

Connect your mobile device with your home Wi-Fi network and use the Wiser app to access and control it.

To pair the device:

IMPORTANT: Before pairing the device, connect your mobile to the home Wi-Fi network.

  1. Open the Wiser app.
  2. On the Devices page, tap Devices.
  3. Tap + (A) to add a device.
    The Add Devices page appears.
  4. The Add Devices page includes the following tabs:
    • Preferred (B): This tab allows you to select a device directly from the preferred list.

    • All (C): This tab includes all available devices for you to select from.

    TIP: You can select a device from either tab based on your preference.
    • Select Preferred > Smart Switch 16Amp (Wiser).

    • Select All > Switches and Controls > Wi-Fi Switches and Controls > Smart Switch 16Amp (Wiser).

  5. Press the push button 4 times in 10 s.
    The LED indicator rapidly blinks green.
  6. Tap Next.
  7. Add the following Device Information:
    • Enter Device Name (D): Add the device name.

    • Assign Existing Room (E): Select an existing room.

    NOTE: If your room is not in the existing room, create a new one.
    • Add New Room (F): Create a new room.

  8. Tap Next.
    NOTE: To begin scanning for devices, make sure to enable Bluetooth permissions.
  9. Tap MAC ID (G).
    NOTE: If you are unable to find the device, tap Rescan (H).
  10. Tap Select Wi-Fi (I) and choose Wi-Fi network.
  11. Enter the Wi-Fi password in the password field.
    NOTE: After entering the password, the Connect (J) button will be enabled.
  12. Tap Connect (J).
    Now, you can see the newly added device on the Devices page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?