Quick (Action)
To create an action:
- On the Actions page, tap Quick.
- Tap + to create an action.
- The Add Action page includes the
following options:
-
Add a Sequence (A): Switch on multiple devices in a sequence.
-
Add Quick Action (B): Switch on multiple devices at a time.
-
- Tap Add a Sequence (A) or Add Quick Action (B).TIP: Follow the same steps to create an action for both Add a Sequence (A) and Add Quick Action (B).
- Tap Add Device (C) and select the device with its respective options from the Devices list (D).
- After selecting the device, tap Done (E).TIP: Repeat steps 5 and 6 to add more than one device.NOTE: You can change the waiting time by tapping the time (F) (Only for Add a Sequence).
- Enter the Action Name (G).
- Tap Icon (H) and select the icon from the list.
- Tap Notification (I) and enable the toggle button for the following options and then tap Save (K):
- Once all the actions are set, on the top right-corner of
the screen, tap Save (J).You can see the newly created action on the Quick page.