DUG_16A Connected Switch-01

Notifications

Notifications allow you to view messages related to your connected devices and keep informed about their status and activities.
  1. Tap Settings.
  2. Tap the Notify Me toggle button.
    NOTE: When you enable the Notify Me button, you can see notification messages on the Dashboard page.
  3. Navigate to a Dashboard page.
  4. On the top right corner of the screen, tap the Notifications (A) button.
    Now, you can see all messages related to devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?