DUG_16A Connected Switch-01

Switching On/Off the device manually

You can switch on/off the device manually. The device will provide power to the electrical appliance connected to it.
Short press the push button on the device once to switch on/off the 16A Switch .

NOTE: It is normal for the front surface of this product to become warm in use.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?