DUG_16A Connected Switch-01

Timeline

The timeline page displays the device’s total energy consumption in kilowatt-hours (kWh) over several time intervals such as the hour, day, last 7 days, month, and year. This allows you to track and analyze your energy usage patterns over a specific time.
  1. On the Devices page, tap Devices.
  2. Select the device.
  3. On the top right corner of the screen, tap Timeline (A).
    The Timeline page appears.
  4. The timeline displays the following options:
    • Live (B): Display the Voltage, Current, Total Energy, Power, Apparent Power, and Power Factor.

    • Hour (C): Displays the total consumption for the selected hour. You can select the time and date by tapping the time and date.

    • Day (D): Displays the total consumption for the selected day. You can select the day by tapping the day.

    • Last 7 Days (E): Displays the total consumption for the past 7 days.

    • Month (F): Displays the total consumption for the selected month. You can select the desired month by tapping the month.

    • Year (G): Displays the total consumption for the selected year. You can select the year by tapping the year.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?