DUG_16A Connected Switch-01

Notifications

The app will send notifications related to your device when you enable the notification button.
  1. On the Devices page, tap Devices.
  2. Select the device.
  3. Tap Settings > Notification.
  4. Tap the Notify Me toggle button to receive notifications.
    NOTE: Tapping the notification icon on the Dashboard page allows you to view all notifications.
  5. Tap Other Notifications. The Other Notifications include the following options:
    • Standby Notification (A): Tap the Standby Notification (A) toggle button to receive notifications when a device is consuming less than the standby value.

      NOTE: The maximum value you can set is 200 watt.
    • Usage Reminder (B): Tap the Usage Reminder (B) toggle button to receive notifications when a device is on for more than the set time.

      NOTE: You can set the time by tapping the time.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?