DUG_16A Connected Switch-01

Voltage detection & load cut-off

This smart feature enables you to set a voltage threshold. When the voltage drops below the set value, it automatically cuts the power supply, thereby protecting the device and extending its lifespan.
  1. On the Devices page, tap Devices.
  2. Select the device.
  3. Tap Settings > Information > Voltage Detection & Load Cut-off.
  4. Drag the green button to set the Low Voltage Cut-off Value (A).
    NOTE: The recommended voltage is 180 V, with a minimum voltage of 90 V and a maximum value of 200 V.
  5. Drag the green button to set the High Voltage Cut-off Value (B).
    NOTE: The recommended voltage is 260 V, with a minimum voltage of 110 V and a maximum value of 300 V.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?