DUG_16A Connected Switch-01

Resetting the device

You can reset the device to factory default manually.

Short-press the push button 14 times (<10 s).
The LED blinks green after 10 s

NOTE: After reset, the device is ready for pairing.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?