DUG_16A Connected Switch-01

Editing a trigger

To edit a trigger:

  1. On the Actions page, tap Trigger.
  2. On the top right corner of the screen, tap .
    The Edit Actions List page appears.
  3. On the Edit Actions List page, tap the trigger you want to edit.
    TIP: If you want the same trigger, tap the hand symbol, it will copy the same trigger and add it to the Edit Actions List.
  4. Tap each item (such as add, remove, rename, etc.) to update.
  5. Once all the edits are done, tap Update.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?