DUG_16A Connected Switch-01

Thermal cut-off value

This smart feature enables you to set a temperature value. When the temperature crosses the set value, it automatically cuts the power supply, thereby protecting the device and extending its lifespan.
  1. On the Devices page, tap Devices.
  2. Select the device.
  3. Tap Settings > Information > Thermal Cut-Off Value.
  4. Drag the green button to set the Thermal Cut-Off value (A).
    NOTE: The default thermal cut-off value is set to 110 degrees.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?