Creating an automation for trigger
- On the Actions page, tap Trigger.
- Tap + (A) to create an automation.
- Tap Add Trigger (B).
- Select a trigger option from the following list on the Select Trigger page:
-
Time (D)
-
Location (E)
-
Device (F)
-
Power (G)
-
Weather (H)
-
- Tap Time (D), select any one of
the following options:
-
Any time: Set for any time.
-
At Specific time: Set for a specific time.
-
At in between time: Set for in between time.
-
Perform only once: Set for only once.
NOTE: Tap the toggle button and then tap Save. -
- Tap Location (E), select any one
of the following options:
-
Arriving location: Select arriving location.
-
Departing location: Select a departing location.
NOTE: Mobile location should turn on. -
- Tap Device (F) and select a device from the list.
- Tap Power (G) and select an option
from the following list:
-
Home EMD
-
Home EMD2
-
- Tap Weather (H) and select an option
from the following list:
-
Outside Temperatures
-
Outside Humidity
-
When Sunrises
-
When Sunsets
-
- Tap Add Device (C) and select the
device with its respective options from the Devices list (I).
- After selecting the device, tap Done (J).
- Enter the Action Name.
- Tap Icon and select the icon from the list.
- Tap Notification and enable the
toggle button for the following options:
-
Show timeline: Displays the total power consumption.
-
Push notifications: Receives the notifications.
-
- Once all the actions are set, tap Save.You can see the newly created automation on the Trigger page.