DUG_16A Connected Switch-01

Customer support

Allows you to contact customer support via email or by calling.

Customer support allows you to address any issues, inquiries, or technical problems users may encounter while using the application. It includes email and direct contact with support representatives, aiming to ensure a positive user experience.

Tap Settings.

Tap Customer Support.

Now, you can contact customer support via Email or by Call.

TIP: Alternatively, you can also navigate to Settings, and on the top right corner of the screen, tap the customer support symbol.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?