DUG_16A Connected Switch-01

Deleting a trigger

To delete a trigger:

  1. On the Actions page, tap Trigger.
  2. On the top right corner of the screen, tap to remove a trigger.
    The Edit Actions List page appears.
  3. On the Edit Actions List page, tap the remove button that is next to the trigger, and then tap Delete to remove it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?