Configure Searches

Configuring searches saves users a considerable amount of time, especially when they repeatedly search using the same criteria. These predefined searches apply to each operational map individually, so you can use configured searches for some operational maps and the default search functionality for others.

Add Searches

By adding and configuring searches, you help eliminate the need for users to select multiple feature layers when performing a common search. Doing so also provides the flexibility of searching on any fields in the designated feature layer; whereas with the default search, only the Display Field for each layer is searched. For example, you may configure a search on the Fuse, Dynamic Protective Devices, and Switch feature layers, called Protected Devices, specifying multiple different search fields for each. Users then need only select that configured search and provide their search criteria.

  1. Click Create.

  2. Type a Display Name (required) that clearly identifies the action of the search.

  3. To add a feature class to your search, click Add New Searchable Feature.

  4. Select a feature from the popup window. You have to include at least one feature.

  5. Click Apply.

  6. For each feature that you add, click the Edit button.

  7. In the Edit Fields popup, click the fields you want in the search.

    The fields you select are populated under the feature.

  8. When that’s finished, click the Save button that is now enabled.

IMPORTANT: As soon as one search is configured for an operational map, the default search functionality is replaced with configured searches. Default behavior returns if all configured searches are removed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.