Run History

The Run History tab displays the execution details of all dynamic workflows. It provides information about a workflow that is currently running, has completed, or has failed. This tab also has buttons indicating the type of each workflow in the list: client dynamic workflow buttons and hosted dynamic workflow buttons.

The Run History is voluminous, especially when you have many users on many different XI series applications. So first, let’s discuss filtering and searching the history.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.