Portal Certificate Download

  1. Navigate to your ArcGIS Enterprise Portal.
  2. Click the lock to the left of the portal URL in the address bar.
  3. Click on “Connection is secure” then click on “Certificate is valid” to view the certificates for the portal.
  4. Click on the “Certification Path” tab, then select the top certificate in the path and click “View Certificate.” Also, do the following for any intermediate certificates. We do not need the last (leaf) certificate in the certification path.
  5. Click “Copy to File…”
  6. Go through the prompts and save your certificate file. Make sure to save the file as Base-64 encoded X.509. Then send the .cer file to Schneider Electric to complete the proxy/HCM setup.
  7. Either upload your certificate in the Client Configuration plugin, or send the certificate attached in an email to ArcFMReadiness@se.com.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.