Sync Settings

The credentials are used for machine-to-machine (M2M) communications when sync is trying to communicate with ArcGIS Server to generate replicas and deltas.

IMPORTANT: Create a Portal account for these M2M communications. Additionally:
  • The Portal account can be the same for Sync Settings and Markup Settings. Or, for more granular access control, use a separate Portal account for Sync Settings and Markup Settings.

  • For Sync Settings, the Portal account must have access to all map services that require offline data.

NOTE: As discussed in the Cybersecurity Best Practices topic in the ArcFM XI Series Architecture Guide, Schneider Electric strongly recommends regularly cycling the M2M credentials.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.