Settings

The Settings area contains high-level configurations for the Solution Center application. These settings apply only to your instance of Solution Center on your local machine, not to all instances across your organization.

There are three configuration choices:

  • Appearance

  • Shortcuts

  • Email Settings


Appearance

  • Background Image

    • Solution Center comes with a default image that can easily be changed. Use the Browse button to locate your image, then click Save. Solution Center supports common image file types such as jpg and png.

    • To restore the image that came with Solution Center, click Reset to default.

  • Icon Scaling

    • To control the default size of the home screen icons, type a scaling percentage. The smaller the percentage, the smaller the icons appear.

      You can also control the icon size using the slide bar on the home screen.


Shortcuts

  • You can assign keyboard shortcuts for each application.

  • Click the Set button, then perform the shortcut. It is automatically saved for the chosen application.

  • Shortcuts currently in use are displayed.

  • Click Clear to remove the shortcut.


Email Settings

You can choose to receive email notifications for Announcements, Dead Letters, and Incidents. For each type of notification, you can further choose which type of Announcement, Product, or Incident status triggers the email. Finally, on the same page, you can Unsubscribe if you no longer want to receive email notifications.

NOTE: You can include multiple emails separated by a semi-colon. The intent is to give you more flexibility on how you want to receive the messages. While the field does accept multiple recipients, it is not recommended to create a group of administrator recipients. Instead, administrators should sign into Solution Center individually and set up their notifications. That way, they can configure their own preferences.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.