Your Services

On the Your Services tab, you are provided with the various Instances of services you host internally. You can refresh the list, view details of each instance, or delete an instance.

If a service is currently running, a green check is displayed next to the name, along with the service version number. If a service is not running, a red exclamation is displayed next to the service name. The list is updated every 3 minutes, and the services report a status every 5 minutes. If a service update has not occurred in 7 minutes, that service is marked as Down.

IMPORTANT: As stated, the service reports its status every 5 minutes. If the service has not reported its status in 30 days, it is assumed to be removed, and it is automatically removed from the list of services.

Click the View Details button to reveal properties of the instance.

The X button deletes a specific resource from the server. However, if the service is still running on that instance, after 5 minutes it re-appears in the list.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.