Queues

All the functions available for Topics are also available for Queues. The only difference is because Queues are structured sequences of events, the only message filter is to choose the Queue Name itself.


Email Notifications

Email notifications are configured in User Options > Settings > Email Notifications. For convenience, the Topics and Queues headers provide a quick link to Open Dead Letter Notifications Settings where you can configure your email preferences.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.