Thumbnail Picture

Thumbnails display next to users’ names if they have an avatar defined through Gravatar.

Users can create an account then set up a thumbnail that syncs with numerous systems, obviously not just ArcFM Solution Center. They can add numerous email addresses that are associated with this particular gravatar.

If the email address exists in Solution Center, then the associated gravatar displays next to the name.

For Corporate and Portal for ArcGIS accounts, if you provide users’ Outlook account emails, Solution Center uses their Outlook profile pictures.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.