Settings

The Settings tab is where you can change the Electric Phase Settings for your tenant.

The Service Bus Connection String can be used to integrate with job services.

The fields on the right indicate the phase designations displayed anywhere within XI series products.

To change your Electric Phase Settings, type the new phase designation in the corresponding field. When you have finished updating the fields, click Save.

If you need to change the default Electric Phase Settings (the phase designations shown in the image above), click the Set Defaults button and all the phase designations are automatically change to the defaults.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.