Incidents

In the event that something goes awry, check the Incidents tab for any open cases that might be affecting users’ devices. The Schneider Electric support team monitors all incidents and immediately posts them here.

NOTE: Any new “high” or “critical” incidents generate a popup message that displays at application launch.

You can Filter by Status {Active, Closed} or Severity {Low, Medium, High, Critical} by using the drop-down lists at the top.


Severity

The following are incident severities and their respective icons:


Email Notifications

Email notifications are configured in Settings on the Email Settings tab. For convenience, the Incidents header provides a quick link to Open Incident Notifications Settings where you can configure your email preferences.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.