Workflow Families

Each subtab on the Default Workflow Studio tab and the Studio tab represents a type of workflow family that corresponds to where the workflows are executed (hosted versus specific client applications, such as Editor, Designer XI, etc.). On the Default Workflow Studio tab, out-of-the-box workflows are provided for each workflow family type. While workflow families have much in common, some have some important distinctions.


More information about workflows and their properties is available in the following topics:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.