Download a Snapshot

Once a snapshot is created, you can download it.

NOTE: This is helpful to transfer snapshots to other machines or servers.

Follow these steps to download a snapshot.

  1. Click a snapshot on the left and view its details on the right.

    NOTE: Use the Search field at the top to find a snapshot by its Title.

  2. At the bottom of the interface, click Download.

    IMPORTANT: There is typically no progress bar displayed, but after a short period of time your local Downloads folder automatically opens when the download is complete.

  3. Notice in your local Downloads folder, the application creates a folder using the GUID of the snapshot as the folder name. Further, it includes all the Assets that were part of the snapshot.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.